This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76925的3.3V供电输出异常



目前问题:3.3V输出基本没啥带负载的能力(用三极管、mos管都用了)。电池组输入到芯片的100欧电阻发烫,三极管烧过一下。

硬件电路如图所示:

电路板焊好之后连电池,PCB中Rbat的100欧姆电阻过热,然后三极管BSR16烧过一次,替换成AO3401MOS管就不烧,但是3.3V引脚的电压只有3.2V,而且输出电流极小,带不动单片机核心板(也就几个mA,龙秋K60核心板)。

将TS1短接后,3.3V引脚输出的电压为3.445V,但是带负载能力明显不足4mA。所测试用的单片机只有两个0805LED,而且基本不亮。

接到后续电路后,3.3V引脚输出的电压只有1.6V左右。

电池组电压22.98V。

求大大带我飞~~