我用TPS54560 作为电源芯片设计了一个DCDC电源板,输入输出用的都是陶瓷电容,芯片背面散热与PCB用焊锡焊牢,故散热应该没什么问题,设计是20~50V输入,5V5A输出。
实际调试后发现,30V输入时,输出只有2A左右(用的是电子负载),用0.1A步进勉强增加到2.2A,再往上增加的话,输出电压就直接掉到1V以下,同时电感有呲呲声。而且测试发现,电压低于15V时,最大输出电流有所增加;输入40V时,最大输出电流约1.7A;输入10V时,最大输出电流有5A(但几秒钟后会热保护,输出电压降为1V以下)。
外围元器件参数均按“TPS54360-361FAMILY_CALC_TOOL_REVE.xls”设计,理论上不应该只能输出这么点功率,求高手指点!!