Other Parts Discussed in Thread: TPS7A30, OPA177
目前想得到一个-5V的基准电压,可以用-12V转化得到-5V吗?
TI的负压LDO TPS7A30指标中有一项Accuracy 为2.5%,它是说明每一个LDO芯片的输出电压在设定值的2.5%上下浮动吗?还是说明不同LDO芯片的输出电压具有离散型,不同芯片的输出电压可能相差2.5%?
怎样理解,盼大神相告!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你说的这两种情况都包括。最恶化的结果是2.5%
-12到-5
电流不大的情况下,可以的
您好,+5v转-5V的运放该怎么选取呢,-5v的基准电压输出电流直接来至运放的输出电流,担心驱动10ma负载时,运放的输出电压会跌落而导致不稳定。我选择20ma输出能力的运放可以吗,带载10ma时-5v能够作为基准电压源吗?
Hi
选择类似上面OPA177的高精度运放即可。
20mA的电流没有问题,供电有电容稳压的,可以作为-5V基准。