This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC2897A有源正激工作几分钟就过流保护。

Other Parts Discussed in Thread: UCC2897A

用UCC2897A做的有源正激工作几分钟后就输入电流变大,触发过流保护了,这是为什么?

  • Hi

        负载没有变动,电流突然变大?

        有没有确认变压器有没有问题? 此时效率是多少?

  • 负载时没有变化的,然后就是变压器比较烫,不过效率方面我的输入18V~36V输出24V带4A负载时,直接采用MOS管作为二极管整流的效率有92.8%。我的用的电流采样变压器做的电流采集,从电流波形来看,变压器在正常工作的情况下是没有要饱和的迹象的。然后就是还有一个问题,有时候会出现带负载不能启动的问题,哪怕是1A电流也不能启动。

  • Hi

        示波器启动测试,cs脚上面确认是否有过流的的信号?(也可能是layout不好,或者滤波效果不好导致CS脚noise较大。)

        其次也怀疑是你的变压器启动时会有饱和的现象,但不很严重,所以稳定下来后看不到问题。

  • CS脚的波形我看了,示波器不加带宽限制会看到一个尖峰,带宽限制20MHZ就没有了。这个尖峰比较接近限流保护的门限,但是任凭我再问呢增大RC这个尖峰始终存在,那么这里的电流限制的信号应该以尖峰为准吗?