打算放电电流30A左右,电量计算精度会下降多少?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这可能需要实际测一下。
但这种场景下,对电流精度影响很大的一个因素是电流检测电阻的温飘。因为在30A时,即使1mOhm的电阻,也有0.9W的功耗,必然会发热很厉害。
电量计有考虑这部分。但电流测量精度导致的误差在这种场景下是比较大的。如果用温飘为300ppm/C的电阻,假设温升是50度。那因为温飘导致的电流测量精度就是1.5%,这部分误差也会引入到电量计算中。