This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC3842驱动变压器,出现电源过流情况

Other Parts Discussed in Thread: UC3842

功能:通过及变压器实现输出电压的放大、频率的增加,通过UC3842实现电流对电压的反馈控制

基本环境:

①输入电压:恒定24V(由直流稳压电源提供,最大电流限制为800mA,默认CV模式)

②只有T1变压器没接上时,UC3842 VOUT信号见下图:最高是24V的矩形波。

③T1变压器接上后,UC3842 Vout波形:

此时,24V电压出现由CV切换为CC模式,24V电压波形也有稳定的24V变为十多V的矩形波

设计电路图见下面:

问题:

1.为什么加上变压器后,输入24V出现过流情况