This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24040 固定10小时安全定时器咨询

Other Parts Discussed in Thread: BQ24040

      根据BQ24040规格书,ISET接2K电阻对地,ISET2接0欧电阻对地,PRETERM电阻设为2K接地,TS引脚接10K电阻对地,序号1 输出端一个只接电池,序号2 输出端接电池和负载并行(负载开机只有45mA);

       在不重新上电、不重新接电池的情况下,长时间静置测试,发现有些问题:

       1. 充电时间超过10小时,BQ24040并没有断开,等待电池电压低于4.05V时就会自动再次充电;

        2.  充电指示灯只有在上电时,指示正在充电,充电满后,灯灭;等下次自动再充电时,指示灯并不会点亮,好像只有上电时指示一次


麻烦你们帮忙解释一下,谢谢!

  • Hi

        TS接10k电阻时,没在TTDM模式下,不会10小时断开。

        The CHG terminal is active low only during the first charge cycle, therefore exiting TTDM or a dropterminalg below VRCH will not turn on the CHG terminal FET, if the CHG terminal is already high impedance.

  • 您好!感谢您的回复

    TTDM模式怎么会10小时断开呢?定时器都禁止了。。。

    Automatic Termination and Timer Disable Mode (TTDM) 

     BQ24040能否用在设置固定多少小时的充电时间,时间到了就永久断开,除非再次断电/上电 或者重新拔插电池才能开启下一轮充电这样的场景?

    谢谢