数据手册里给出的测试条件是“VBAT = 4.2 V, boost mode,I(VBUS)= 0 A, converter switching”,这指的是没有充电和负载的情况下,系统的静态电流吗?BQ25895对应的电流是5mA,会不会很大?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
这里是指工作在boost时PMID 5V输出, PFM_OTG_DIS=0 典型值是3mA, 没有最大值,5mA不算很大。
可以测试一下测试电池的电压是否准确的是4.2V, 以及以及确认测试仪器的准度。(如果是用电流表串进去造成路径较远可能是有影响的。)