BQ24610 的BATFET在电池充电时时打开的,那么在电池充满电后的状态时什么样的?
另外TTC那个脚时用来设置定时器和终止控制的,,,不明白定时器和终止时用在哪里,这个脚的设置会影响芯片的什么功能,可以解答一下吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
见datasheet描述:
The device will terminate charging when the termination current threshold has been reached and will begin a recharge cycle when the battery voltage has dropped below the recharge threshold (VRECHG).
当充电电流小于the termination current threshold, 充电就会停止。(BATFET关闭)
As a safety backup, the bq2461x also provides a programmable charge timer. The charge time is programmed by the capacitor connected between the TTC pin and GND,
定时器的作用在于安全方面,例如你设置3小时充电,那么3小时候后自动停止充电。防止一些电池异常造成的安全问题之类。