This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

uc3875移相问题



 TI官方,您好,这是我用37875的外围电路,我现在做的是电压单闭环控制,其中PI参数为才C1=47NF,R1=49.9K,C2=100PF.当采样电压达到基准时,pwm波跳动的太厉害了。 蓝色为超前臂的下桥臂Q3,绿色为滞后臂的上桥臂Q2,红色为pin2脚输出。

请问:

1、移相怎么会出现Q3这样的波形,这是移相吗?

2、需要确定移相是OUTA,OUTB为基准,OUTC,OUTD相对移动产生移相吗?

3、外围电路连接有问题吗?可改进的有哪些?

  •  按理来说,IC输出的应该是占空比接近50%的方波啊?而且如果是IC输出的应该只有正信号或者零,你的绿色怎么还有副值?你确定你测量的是IC输出的信号,而不是MOS管的驱动信号?

  • 回答:

    1、IC输出是占空比为49.5%的方波,之后我把死区加大,占空比大概在46%。

    2、所测的为IGBT  GE两端波形。

    我的问题是为什么移相的时候蓝色的占空比会变,不是移动吗,怎么改变占空比尼?