This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq51050关于无线充电和有线充电的切换问题

Other Parts Discussed in Thread: BQ51050B

问题1:使用bq51050b芯片给锂电池充电时,无线充电和有限充电功能切换,下面两种观点哪种是正确的:

第一种观点:当给EN2引脚施加高电平时,即EN2=1时,无线充电使能,BAT管脚输出电流对电池充电;有线充电禁止。

                        当给EN2引脚施加低电平时,即EN2=0时,无线充电禁止,BAT管脚输出高阻抗;有线充电使能。

                        即切换完全由EN2引脚电压决定。

第二种观点:

                        当EN2=0时:
                                              如果AD管脚输入电压大于3.6V,那么有线充电使能,BAT管脚输出高阻抗。
                                              如果AD管脚输入电压小于3.6V,那么无线充电使能,BAT管脚输出电流对电池充电。
                        当EN2=1时:
                                              有线充电被禁止,无线充电总是使能,BAT管脚输出电流对电池充电,此时AD管脚上的电压不起作用,AD-EN输出高电平。

                       即切换是由EN2和AD两个引脚电压共同决定的。

问题2:我设计的无线充电电路,测量电池温度的ntc电阻信号是传给cpu的AD引脚的,当cpu检测这个信号并发觉电池温度过高,便通过控制bq51050b的EN2的引脚来将无线充电状态切换到有线充电状态(实际电路并未设计有线充电),以使BAT管脚输出高阻抗,禁止输出电流给电池充电,以此达到过热保护。这种方法正确吗?