Other Parts Discussed in Thread: UCD9222, UCD7242
您好,我按照6678EVM开发板设计了相同的ucd9222+ucd7242的电源组合模块,通过usb to gpio连接器连接上电脑后,运行fusion digital gui软件的online模式,识别了该器件。gui软件是2.0的版本,我看了下,使用方法和官方提供的1.8版本的教程不太一样。对于新的9222芯片,连接并识别后,可以选择通过已有工程导入,我试着导入6678evm开发板上的9222的电源gui配置工程文件,得到图片所示的结果,测量发现,两路电压都未出来。我又尝试导出烧录程序,用该套软件的DOWNLOAD插件烧录,发现并不能导出教程中所给出的“.x0”格式的烧录文件,并且另外两种格式的文件“.hex”和“.srec”格式烧录均失败。我不太清楚是哪个环节出了问题,就试着用6678EVM开发板试着连接了一下GUI软件,运行online模式,发现一样出现图片所示的结果,并且在该过程中,两路电压也都没了,但是断开pmbus连接重新上电后,两路电压恢复。由于开发板还要用于部门其他同事的软件调试,因此并不能尝试清除ucd9222内存进行烧录的试验。我手边关于该电源组合的配置教程都是基于官方的1.8版本,但是现在TI官网下载不到1.8版本的GUI软件,也不能找到2.0版本的相关教程,在尝试以上操作多次后均不能正确配置电源管理模块,想请大神帮忙,看看是否有操作失误的地方,并予以指教,谢谢!