Other Parts Discussed in Thread: LM1085, LMS1587, LMS1585A, LM1084, TPS62130A, TPS7A84, TPS7A47
需要大功率,电流可以在3A左右,输入12V电压,输出D5V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LM1085和LMS1587(Iout=3A),noise:38uVrms
如果会长时间超过3A,建议使用LM1084和LMS1585A(5.5A)
这两款的主要区别在于输入和输出电压范围
输入12V,输出5v,压差是7V,电流是3A。
也就是说在LDO的上热耗是21W。
热耗太大了。
Hi
不建议直接用LDO, 如果对于输出的要求非常高,可以采用DC/DC + LDO (或者LC滤波器)
21W的功耗除了散热设计非常麻烦之外,还费电,效率太低。
DC/DC 可以选择TPS62130A这样的同步芯片,输出设计5.5V,
LDO可以选择TPS7A84, 5V输出,输出噪声 7.7 µVRMS (另外如果你的要求没有这么高,你可以选择一些较低Vdorp的LDO, 效率还会再高一些。)
Hi
超过1A都这样建议,只是你可以选择不同的DC/DC和LDO.
1A以下,如果你不介意效率,可以直接选择LDO, 如TPS7A47 4.17uVrms.
能不能再推荐个输入VDD12V输出VCC11V的低噪声芯片啊,谢谢
HI
电流多大? 如1A以内,上述推荐的TPS7A47就可以。