This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24072使用咨询

Other Parts Discussed in Thread: BQ24072, BQ24075

手持式设备想要一颗带电源路径管理的芯片,已保证在设备工作的时候能够充满电,现在选型初步定为BQ24072,有几个问题想咨询下:

1.BQ24072 VOUT(REG)输出为VBAT+225mv,VBAT(REG)输出为4.2V

当充电电源未接,只接锂电池,此时VOUT=VBAT电压

当接上充电电源,锂电池未接,此时VOUT是什么值?是4.2V?

当接上充电电源,锂电池也接上,锂电池在充电,此时VOUT输出是多少?是VBAT+225mv?如果这样的话,那么这个时候电池的充电电压也不是4.2V了

2. 这款芯片能支持的最大充电电流为1A,有测试过当达到多少的时候芯片就比较烫,毕竟有0.8V的压降,当500ma的充电电流时就会有0.4W的损失

谢谢!

  • 另外补充一个问题

    BQ24075上使用的SYSOFF这个管脚究竟在什么情况下可以用到,有什么好处

    谢谢!

  • Hi

         1. 从你的描述看你并没有接系统负载,所以当充电电源未接,只接锂电池,此时VOUT=VBAT电压(否者就会有一个压降,充电MOS)

         接上充电电源,锂电池未接,此时VOUT是可能是3.4V(接负载,具体你看可以测量确认)。当接上充电电源,锂电池也接上,锂电池在充电,此时VOUT输出是VBAT+200mV.  所以Vout是变化的,并维持最低3.4V供电给到系统。

        2. 芯片烫是因为你的layout没有做好,这个芯片的热阻不高,注意芯片底部的Power需要打孔到中间层或者底层的GND, 用于散热。

        3.  主要针对电池没有安装的情况。