看了手册,感觉BQ76940在成本,性能上有优势(BQ76BL455不考虑,成本不允许),求教BQ76940能不能采用某种方法级联,来应用在24S-30S的系统中?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可以参考Industrial Battery Management Module for 20S Applications Reference Design。这是两个BQ76930级联的方案。
http://www.ti.com/tool/TIDA-01093?keyMatch=bq76930&tisearch=tidesigns
Description
High serial cell count battery (>15s) systems are becoming more and more common for industrial applications. These applications are cost sensitive and require a simple solution that includes monitoring, protection, and control or even SOC (State of Charge) information rather than only basic independent hardware protection. This design offers a platform for the complete pack side solution. All independent hardware protection features are incorporated from the bq76930 and a robust communication interface is implemented for host device to read the battery information.