我想单独使用EMB1428Q进行电池主动均衡设计,EMB1428Q用于开关矩阵的驱动,但是有一些问题想咨询一下
我想做的方案是将电池组分成几个模块,每个模块的开关矩阵采用贵公司的方案,开关矩阵右边是双向变换器的一边,以此实现任意两个模块中的任意两个单体电池之间的均衡。但是对于EMB1428Q驱动芯片有一些疑问:
1.EMB1428Q是否可以将Vstack连接到电池组内单个模块中的最顶端电池的正端?如第二张图红线所示,这个个人感觉是可以的;
2.EMB1428Q的GND和GNDP是否可以直接连接在每个电池模块中最底端电池的负端,如第二张图红线所示,这个个人感觉是可以的;地之间的连接是否要单点连接?
3.VDD12V,VDDP,VDD5V,VDDIO是否都可以直接与每个模块最底端电池的负端通过解耦电容相连?在这种应用情况下,这些端口是不是每个都需要供电?
4.单独使用的时候,EN是否与DONE直接相连就可以了?DIR与/DIR是不是直接相连就可以了?三个FAULT直接连接到每个模块最底端电池的负端?就如第二张图所示?
5.因为模块间需要隔离,对于各个模块的SPI通信接口,是否可以通过数字隔离芯片直接连接到MCU的SPI接口?
6.因为SPI总线只有一条,对于任意两个模块中的电池单体之间进行均衡的情况,是否可以通过SPI先对其中一个模块的EMB1428Q进行控制,使得该模块开关打开,然后将该模块芯片的CS片选信号置高,再将另一模块的CS片选信号置低,操作另一模块的EMB1428Q,控制另一模块的开关。也就是对于每个EMB1428Q,只需要写入一次命令就可以,而不需要一直占用SPI总线,是吗?
7.每个芯片的功耗预计有多高?