This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1应用场景问题

Other Parts Discussed in Thread: BQ34Z100-G1, BQ34110

您好,

        对于BQ34Z100-G1应用于铅酸电池容量测量,我想请教以下问题:

1.对于一组电池完成学习过程,即完成更新QMax和Ra table值。将量产芯片启用IT算法,应用于长期处于浮充状态(电流不为0)且极少放电的情况下,

电池容量的测量,随之电池使用时间增长,Ra table值内阻值能更新么,什么时候更新?

是否芯片一直保持的是学习过程完成时的Qmax和Ra table值?一年,三年或者五年之后内阻值相较于最初的状态肯定有变化,怎么保证之后测量一年,三年或者五年之后的容量测量准确度,是通过充放电过程么?

2.BQ34Z100-G1的健康值显示为预测的FCC/design capacity,这个健康值的更新,对于长期处于浮充状态(电流不为0,但是极小)且极少放电的情况,是不是没有效果?

BQ34Z100-G1怎么保证预测的FCC的值的准确呢?

期待您的回复,谢谢!

  • 34z100并不适用这样的条件。 

    建议参考bq34110,针对极少放电的电池的寿命估算电量计芯片

    Multi-Chemistry High-cell Count Battery Fuel Gauge w/Integrated Rarely Discharged Module

  • 您好,

           BQ34110适用于极少放电的铅酸蓄电池的容量及寿命估算,在什么样的条件下能够进行容量及寿命估算呢?

    1.必须有一个完整的充放电循环么?即充满电,放电到截止电压的过程。

    2.我想问一下,这个极少放电的应用场景,指的是平时一直都是放电出极少部分的电量,从来不会放电到截至电压呢?

    还是指平时除了自放电外不加任何负载的不放电,但是需要有放电放到截至电压(即放出100%的电量)呢?

    3.BQ34110是只需要进行一些参数配置就能直接应用于终端产品(铅酸蓄电池组)的容量及寿命估算么?

    如果不是,那么BQ34110的工作过程是怎样的呢?需要提前做哪些工作呢?

    期待您的回复,谢谢!

  • 同求工作过程,及读取数据流程。