This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EMB1428Q进行分组的多节电池的主动均衡的使用问题

不知道是不是之前的图不清晰,至今没有回复,在此将AD的原理图附上,进行问题阐述。

图在下面

我想做的方案是将电池组分成几个组,每个模块的开关矩阵采用贵公司的方案,开关矩阵右边是双向变换器的一边,以此实现任意两个模块中的任意两个单体电池之间的均衡。但是对于EMB1428Q驱动芯片有一些疑问:

1.EMB1428Q是否可以将Vstack连接到电池组内单个模块中的最顶端电池的正端?

2.EMB1428Q的GND和GNDP是否可以直接连接在每个电池模块中最底端电池的负端?

3.VDD12V,VDDP,VDD5V,VDDIO是否都可以直接与每个模块最底端电池的负端通过解耦电容相连?在这种应用情况下,这些端口是不是每个都需要供电?

4.单独使用的时候,EN是否与DONE直接相连就可以了?DIR与/DIR是不是直接相连就可以了?三个FAULT直接连接到每个模块最底端电池的负端?

5.因为模块间需要隔离,对于各个模块的SPI通信接口,需要通过数字隔离芯片连接到MCU的SPI接口,而SPI总线只有一条,对于任意两个模块中的电池单体之间进行均衡的情况,是否可以通过SPI先对其中一个模块的EMB1428Q进行控制,使得该模块开关打开,然后将该模块芯片的CS片选信号置高,再将另一模块的CS片选信号置低,操作另一模块的EMB1428Q,控制另一模块的开关。也就是对于每个EMB1428Q,只需要写入一次命令就可以,而不需要一直占用SPI总线,是吗?