This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25895 PMID输出电流设置问题

Other Parts Discussed in Thread: BQ25895, BQ25890

Dear TI:

在产品中使用BQ25895给3000mAh 1S锂电池充电,输入电压VBUS为5V。当移除VBUS,采用BOOST模式时,希望PMID电流设置为1.65A。

1、请问采用BQ25895能否设置?(REG0A寄存器低4位为Reserved)是通过什么方法设置的?

2、BQ25890 REG0A的低3位可以设置Boost Mode Current Limit(Default 1.4A),我在BQ25895上设置该3位发现PMID输出电流会有明显变化,正常来说BQ25895是不支持该寄存器设置的,请帮忙分析?

  • Hi

       这个电流应该是没有办法限制到1.65A的。

  • 1、请问采用BQ25895能否设置?(REG0A寄存器低4位为Reserved)是通过什么方法设置的?

    无法设置。不带输出恒流(限流)功能。

    2、BQ25890 REG0A的低3位可以设置Boost Mode Current Limit(Default 1.4A),我在BQ25895上设置该3位发现PMID输出电流会有明显变化,正常来说BQ25895是不支持该寄存器设置的,请帮忙分析?

    BQ25890和BQ25895的应用场景不一样,这个current limit设置的在boost模式下VBUS(不是PMID)作为输出口时的电流限制。如果用BQ25890的PMID作为输出,跟BQ25890一样,没有输出限流功能。