This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于BQ24172充电问题



针对两节8.4V锂电池充电,输入12V的适配器。

原理图如下:

 

PCB图如下:双面板,单面放器件

可以正常使用,但是经常容易坏,输出只剩下0.8V,重新换芯片可以正常使用。什么问题会超成这种这种情况,目前已进入量产,但是这个不稳定,超成很多不良率。

希望能帮我找出问题所在,谢谢!