各位TI的专家大神们:
最近有个12串 10-12并 45.6V 200A的电池项目,有没有推荐的电源管理芯片呢?另外BQ76940是否能满足要求呢,主要是电流是否满足,能否检测到这么大的电流呢?
非常感谢!~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位TI的专家大神们:
最近有个12串 10-12并 45.6V 200A的电池项目,有没有推荐的电源管理芯片呢?另外BQ76940是否能满足要求呢,主要是电流是否满足,能否检测到这么大的电流呢?
非常感谢!~
Hi
电源部分下面方案或许能帮到你: http://www.ti.com/tool/TIDA-00364
BQ76940可以的。电流采样走的是电阻,芯片关注的是采样电阻两端的电压,只要在芯片范围内就OK.
你好,你是说推多个MOSFET并联,比如24个,可以用这个FET驱动器吗?
因为我这边的案子都是大电流的,包括叉车、堆高车和低速四轮,MOSFET采用100V以内的,FET驱动这块目前都是采用PNP+NPN图腾驱动,不知道用你给的这个方案加以修改是不是比PNPNPN图腾驱动会好很多?
目前我采用的都是继电器方案,但功耗功耗较大,成本较高,且装配麻烦,但多管并联的fet驱动不好设计(通常我做的要达到200A持续 600A脉冲的)
如果是这么多MOS并联的,BQ769X0可能不合适,因为放电管的关断电流不大,在做短路实验的时候,可能造成MOS损坏。
使用外加驱动是可以的,在驱动信号和MOS之间放一个low side驱动即可。