This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24232充电指示灯不熄灭问题



电路如图,NTC使用10K电阻暂时替代。电池为聚合物锂电池,200mah。

电路是按照WEBENCH取值的。

现在情况如下,输出正常,充电输入5V。

充电输入连上之后(5V@110ma左右),两个LED同时亮,充了很久很久(6小时以上),俩LED都不会熄灭,电池电压测量已经到达4.22V,充电电流仅剩6ma,但是LED还是亮着。

Vout端空置 无负载。

焊接了两块电路板 都是一模一样症状。。。

现求助各位dalao,小弟不知道为何会这样