根据TI手册是写的,只需要更改FB引脚的电阻比值就可以输出12V电压,那power good 引脚应该接在输入端还是怎么处理?芯片手册并没有给出具体的电路,我参照了前人的设计,发现有些是接在输入上的,有些是悬空的,请问到底该如何处理?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
电路图你可以通过TI的仿真软件webench得到,只要输入相关参数,即可得到电路以及电路的相关参数,如效率温升等,见芯片网站:
http://www.ti.com.cn/product/cn/LM25011
Powergood可以接任何低于7V的稳定电压源(一般要看Powergood对应的接口电压范围选择电压源,例如接口是3.3V, 并且不能承受7V,你就只能选择3.3V左右的电压源。)
LM25011 --具有可调节电流限制的 42V、2A 宽输入电压恒定导通时间的开关稳压器。
推荐使用http://www.ti.com.cn/product/cn/lm25011上的 WEBENCH® Designer LM25011 进行设计。
PGD引脚功能如下:
| PGD | – | Power Good | Logic output indicates when the voltage at the FB pin has increased to above 95% of the internal reference voltage. Hysteresis is provided. An external pull-up resistor to a voltage less than 7 V is required. |
电压应低于7V