最近在看TPS5430产生负电压的电路图,我发现datasheet给的都是-5V的原理图,本来我打算改为-12V输出的,但是我发现一个问题,FB反馈回来的电压,与REF电压一起控制PWM的占空比,那么,不久是固定了输出只能为-5V吗?这样就不能改变输出为-12V了吗?因为要将反馈回来的电压设置为REF,才能达到相对稳定,不是吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最近在看TPS5430产生负电压的电路图,我发现datasheet给的都是-5V的原理图,本来我打算改为-12V输出的,但是我发现一个问题,FB反馈回来的电压,与REF电压一起控制PWM的占空比,那么,不久是固定了输出只能为-5V吗?这样就不能改变输出为-12V了吗?因为要将反馈回来的电压设置为REF,才能达到相对稳定,不是吗?
分压电阻R1和R2的作用就是保持VSNS脚等于内部参考电压,只要调整分压电阻比值,保证在-12V时,VSNS脚电压等于内部参考即可。
TPS5430 VSNS脚为1.221V。使用分压电阻进行相应计算即可。
Hi
用buck芯片shift GND变成buck-boost拓扑,芯片的GND的电压从0V下移到负电压(如你要的-12V), 但有一样没有变,那就是电压反馈中基准电压与芯片GND之间的压差。
-12V 参考方案: http://www.ti.com.cn/tool/cn/pmp2224
如果参数有差异,你需要参照你看到的-5V设计文档,修改这个设计。