Other Parts Discussed in Thread: TPS62293
尊敬的TI工程师:
您好!我们在使用TPS62293时遇到问题,我们采用的芯片电源输入为+5V,芯片输出1.8V电压,但是在做实验时发现,1.8V有间歇掉电的情况,1.8V输出是给我们使用的FPGA K7325T供电的,1.8V间歇掉电引起了K7325T的重新加载,最终导致我们的产品工作异常,附件中的“1.8V掉电毛刺”是示波器捕捉到的1.8V掉电的瞬间和宏观图,图中黄色信号为1.8V, 绿色信号为指示FPGA重新加载的DONE信号,发现在1.8V变低后FPGA重新加载,表现为DONE变低,之后系统工作异常。麻烦您帮我们分析一下可能的原因,是什么导致的1.8V间歇掉电,找到原因的话采用什么改进措施可以解决此问题,谢谢!不胜感激!