Other Parts Discussed in Thread: LM46002
LM46002 加0.6A以上负载 然后通电 出现保护 输出电压不正常。
24V输入 3.3V输出,先加负载(0.6A~2A),然后通电,输出电压不正常,应该是出现保护(输出电压为0,去掉负载,输出电压立马正常)。
如果先通电,后加负载,负载可以加到2A,输出都很正常。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LM46002
LM46002 加0.6A以上负载 然后通电 出现保护 输出电压不正常。
24V输入 3.3V输出,先加负载(0.6A~2A),然后通电,输出电压不正常,应该是出现保护(输出电压为0,去掉负载,输出电压立马正常)。
如果先通电,后加负载,负载可以加到2A,输出都很正常。
Hi
首先确认你的电感饱和电流必须大于2.2A以上。
其次确认你的layout, 注意功率路径尽量小。 (如果是东东板面包版之类的,带载能力大幅下降是正常的,layout对于电源而言非常重要)
状态1:先通电 后加2A负载,输出正常。
状态2:先加载,后通电,输出不正常(负载不去掉或者负载不降到0.6A,一直无输出)。有点通电瞬间保护的现象。
如果是layout有问题,那么两种状态都应该不正常啊!
在状态1时 用示波器测量 开关节点SW脚 输出频率和脉宽都很稳定,频率为500KHZ左右。
在状态2时 用示波器测量 开关节点SW脚 有波形(说明芯片已经启动并工作) ,但是波形很不稳定,
输出频率变成110KHZ,脉宽变的更窄,同时用示波器补捉输出波形无电压(0.5V电压)。