Other Parts Discussed in Thread: LM2663
做的是光电二极管的放大和滤波电路。用lm2663将5V转为-5V,已单独接地,但还有几十mV的15kHz及高频谐波干扰信号,如何去除呢?运放电源端接的是10uF钽电容和0.1uF陶瓷电容,另,运放和LM2663需在同一块板上。。。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
这个可能是芯片内部开关造成的,建议你将输出改为2个10uF陶瓷电容看看效果。
对于要求很高的运放和滤波电路,建议采用高PSRR超低noise的LDO, 或者在你现在电路基础上再增加一级LC看看能否满足要求。
layout也是很重要的,包括你提到的GND,你需要注意。