This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDO和DC-DC如何做选择



输入5v,可以输出3.3v或2.5v或1.2v,在选择LDO或者DCDC器件时候,选择其中一种时候该考虑哪些需求?

  • Hi

       选择LDO,  优势在于电路简单(没有电感),占用空间小,成本相对较低,纹波noise都很小。劣势在于效率非常低,特别是压差比较大时,例如1.2V时效率只有24%.

       另外最大输出电流相对比较小,在电流比较大时间,压差也比较大时,芯片功耗特别大,散热设计很麻烦。

        选择DC/DC, 很多则相反,有电感,占用空间大,成本相对较高,纹波noise相对较大。 但是优势在于效率比较高,很多芯片都可以做到95%左右。输出电流也可以做到比较大,即便压差大,功耗也不是很大,散热设计简单。