This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于LM7805反向输入的问题



我们知道LM7805为三端稳压器件,1脚输入,2脚地,3脚输出。

在使用过程中,发现当2、3脚间加激励后,1、2脚有输出,而且,只有2、3脚间有电压,1、2脚间就有输出。最小测试,0.5V输入,输出为0.4V,之后线性递增。

当然这是一种错误的使用方式,但是,想请教一下各位同仁,发生这种的情况的原理是什么?是其内部三极管阵列被击穿嘛?

这种反向输入的情况,芯片的能耗很大,芯片很热。但是一段时间后,按正确接法,器件还能输出稳定的5V。

请问,反接情况下,输入管脚间,有电压输出的原理,以及可能对芯片造成的损伤。谢谢。

  • Hi

          见datasheet第十三页描述: 

          Because the output of the device does not sink current, forcing the output high can cause damage to internal low current paths in a manner similar to that just described in Shorting the Regulator Input.

         这一页说得比较详细,如果输出电压高出输入(包括你提到输出有电压输入没有)是会存在烧掉芯片的风险的,是要避免。

         芯片内部并无通路,输入有电压很可能芯片已损坏。

         

  • 为了防止输出高于太多造成IC损坏,所以三端稳压器一般在输出到输入接一个二极管。