This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用LM27313作为升压芯片IC,输入大概在7V,输出8V,关断管教接3,3V电源,再下拉到地,
正常工作时,一切正常。
当/SHDN近0V时, 输出依然有6,5V的电压,并且至少有100mA的驱动能力。看起来关断功能失效,请问该问题该如何解决?谢谢!
建议你再确认下SHDN引脚电压及电流,datasheet中给出的Device OFF阈值上限最大为0.5V。
我测量过,的确是在门限以内。
TPS62160为降压型DC/DC,也有类似问题,明明已经关断,其输出不为零。
如果不带再负载,倒是正常。带负载有问题。