Other Parts Discussed in Thread: TPS54260, TPS54160
1、TPS54260是降压性电源芯片,手册以及其他资料SLVA369等给的例子都是由高电压向低电压转换的,是不是说这个芯片不能进行升压操作。比如输入+12V输出 ±12V,或者输出 ±24V等等。
2、TPS54260手册中的Figure 64 Split-Rail操作原理图中有个Lo,这个Lo是个变压器吗?我计算出来Lo=135uH,我是选择哪种大的变压器还是选择普通电感就行了
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
TPS54260是降压芯片,顾名思义只能做降压转换(输出电压必须比输入电压低),可以设计成为buck-boost输出负电压。
是变压器(耦合电感),一般不会用这么大的感量,计算方法参照: http://www.ti.com.cn/cn/lit/an/slva369a/slva369a.pdf (可以调节频率等参数让感量小一点,如果电流很小可以用小电流版本的芯片)
TPS54160是TPS54260的1.5A输出版本。
我的目的是输入+12V,输出±12V,±15V,±24V,比24V再高点也可以。输出电流最大2A-3A。请问有没有合适的芯片或者方案推荐
有没有可以实现上述电压的方案,输出电流最大1A-2A或者2A-3A