Other Parts Discussed in Thread: UC1823, UCC27714, UCC29910A
请问有UC1823 BUCK电路的参考设计吗?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这个芯片比较老了,没有合适的参考设计。你的功率很大么?如果是小功率应用,可以用TI的webench选择高集成度的buck芯片。
Hi
具体输入输出规格?是否仍需要时军用级别的芯片?
工作温度:-20℃~+125℃连续工作250小时以上;
如果电流不太大,用一颗UCC29910A,如果电流比较大,用UCC29910+UCC27714(高压驱动)来做即可。