This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI3354+锂电池供电问题!



各位大侠,目前在做一个产品,采用TI3354+锂电池供电,3354供电采用TPS65217C芯片,现在出现了这么一个问题,当锂电池电压低到一定的时候,发现系统关机了,而且你将外部电源插上去,系统也不工作,一定要把锂电池拔了,在插上外部电源,系统才能起来,在不拔锂电池的时候,发现给TPS65217C供电的电压还是有电压的,而且之前捕获过,在系统关机瞬间,给TPS65217C供电的电压有一个下降,但马上又抬回去了,但系统不工作了!根据这个现象应该是锂电池在这个情况下,供电不足,出现电压下降,导致系统关机,系统关了之后,负载降低,电压又上来了!但此时是不是TPS65217C电压管理的问题?不知道,各位是否有遇到,或者有什么好办法解决???

  • 这边在看了TPS65217C的手册,发现有这么一段话:To enter OFF state, set the OFF bit in the STATUS register to ‘1’ and then pull the PWR_EN pin low. Please note that in normal operation OFF state can only be entered from ACTIVE state. Whenever a fault occurs during operation such as thermal shutdown, power-good fail, under voltage lockout, or PWR_EN pin timeout, all power rails are shut-down and the device goes to OFF state. The device will remain in OFF state until the fault has been removed and a new power-up event has occurred.

    红色标识的应该就是我这个电压问题吧,这边需要新的power-up event ,也就是重新上电的过程,但锂电池这边电压马上就上去了,所以没有这么个过程,就一直保持在OFF的状态了,应该是这么理解吧,

  • 设置TPS65217C的放电截止电压大一些,即避免进入欠压模式看是否能解决这个问题。