This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5520疑问!



 2:VDDIO,只需接MCU的一端口?   
        开关机是否需遵守上下电时序?
         在低功耗和唤醒时,要满足时序要求,芯片的电源需加MOS控制开关?
         如下图:
3:复位端无时序图,在MCU端口不够的情况下,能否用阻容复位?
     还是一定得用MCU的IO口输出?
  • Hi

       1.  7.3.1 Start-Up Powering VDDD and VDDA must be tied together and turned on first. VDDIO must be turned on at the same time as VDDD or later. In the power-off sequence VDDIO must be turned off before VDDD or at the same time.

       2. 能符合电平变换要求即可, 正常接高。

         

  • 1:那可完全按参考设计接法(I2C模式下),不需要用MOS管去开关电源即VDDD,VDDA ?

    2:延时需10us ,但未描述是低还是高电平复位?

         参考设计是接MCU的IO口,你说直接接高,是接电源?

        那是按参考设计接IO口还是按你说的接电源?是否可用阻容方式延时10us 以上?