This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB快充协议5V/2A实现方式



问一下,做一个USB快充5V/2A的实现方式需要外加USB快充协议芯片么,如果需要,有什么廉价的方案推荐么。

还是说能否不要外部协议芯片,直接D+给0.6v电压,D-接地就可以协商到5v/2A供电了呢,谢谢。

我想做一个USB快充的方案,前端只能出5V,后端支持可以上2A的电流,不支持快充的时候给1A的电流。

小弟最近才接触这一块不是很懂,希望有大神解释一下,谢谢。