This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq40Z60不工作

Other Parts Discussed in Thread: BQ40Z60, EV2400

目前用的bq40z60,用的是电池包,电池包里有保护板,共三个电芯。接法是电池包的正极直接接入VC3。GND与VC1,VC1与VC2,VC2与VC3之间各串了一个1K的电阻。电源适配器用的是DC15V.
bq40z60的外围电路检查过,与示例电路几乎完全一致,应该没问题。
芯片是TI代理给的样品,以下所有情况都确定VCC是有电压的。故障现象如下:
一开始芯片完全不工作,但是测到ACP为15V。REGN和PBI没有电压,
后来通过EV2400配置了一些参数后,目前ACP用示波器测到的适配器电压在19V,15V,10V三个电压间循环规律跳动,配置前是15V。但是用EV2400在软件界面上监测到的为6.7V。
LODRV和HIDRV现在用示波器观察到有振荡波形输出,但是这两个用万用表依旧测到0V,万用表也还是测不到PBI和REGN有电压。
现在相当于ACFET HIDRV LODRV DSG CHG几个驱动MOS的引脚都没打开。请问如何配置,才能让这个芯片正常使用起来。

邮箱9431242989

电话13760174171

深圳普门科技有限公司