求一款电源芯片输入9-15V,输出5V,限流20mA>>>>>>>>>>不知道有没有这样的芯片>>,如果采用电源管理芯片怎样可以实现?求大手们告知
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
求一款电源芯片输入9-15V,输出5V,限流20mA>>>>>>>>>>不知道有没有这样的芯片>>,如果采用电源管理芯片怎样可以实现?求大手们告知
Hi
找可调或者可控过流保护的芯片即可。TI大部分芯片过流保护都是内置的,如果外置一般电流还是比较大的,设置20mA的过流保护芯片不是很好找。
TPS62122, 75mA,有过载保护,大约在250mA左右出现保护。
你也可以自己通过WEBENCH进行芯片选型
20mA限流保护的芯片没有,需要你自己加外围电路实现。