This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

控制芯片咨询

Other Parts Discussed in Thread: UCC25230

针对以下的条件,您是否有相应的电源管理芯片:

Input  24±20% VDC

Output1   12VDC  100mA

Output2   12VDC  100mA

输入输出隔离。两路输出隔离。成本低,成熟的方案,如果方便的话,能否电话沟通,利于交流,非常期待您的答复

  • 您好,推荐您使用TI的UCC25230,该芯片应用在FlyBuck拓扑中,可以实现隔离的两路输出。该芯片无需辅助绕组,变压器只有原副边两个绕组,成本低易于设计;UCC25230具有过压和欠压等保护。

    如需更详细的信息,可以邮件我,谢谢。Neil-li@ti.com

x 出现错误。请重试或与管理员联系。