1.测试电路板:TPS63070官方DEMO,型号为TPS63070EVM-693

2.输出电压:5V(VSEL引脚接高,输出电压为5V)
3.输入电压:9.8V,确定芯片工作在BUCK模式下
4.PS/SYNC引脚接低电平,强制芯片工作在PWM模式
5.负载:大功率电阻,5欧姆/50W
6.测试过程:
a.空载启动,输出电压为5V,电源芯片工作正常;
b.带负载启动,输出电压为3.0V左右,输出电压不正确,电源芯片工作不正常。查看上电过程中输出电压波形,电压上升到3.85V之后下降到2.9V后稳定。
此时L1引脚波形如下,方波占空比30.7%,符合9.8V输入,2.9V输出条件.
c.空载启动成功之后——即PG引脚输出高电平之后,再带电接入负载,输出电压基本不变。也就是上电成功之后,再将负载电流从0A上升到1.25A,输出电压基本不变,符合芯片手册中负载传输相应曲线
d.将VSEL引脚接地,输出电压为3.3V。此时带负载启动,输出电压为3.3V,输出电流0.825A。芯片正常工作。
e.将VSEL引脚接地,输出电压为3.3V。此时将负载电阻改为2欧姆/50W,计算输出电流1.65A。此时带载启动,输出电压降为为1.8V,电源芯片工作不正常。
7.分析:
从第6项的a-c测试,基本可以分析到,1.25A负载条件下,芯片的启动过程收到影响。查看芯片手册,图表17和19分别描述了输出电压为7V和9V的情况下输出电流的大小,可以读出10V输入电压时,输出电流最大为0.88A和0.78A。我理解这表示输出电流大于这两个数值的情况,会影响芯片的正常启动,所以此时芯片输出不正常。

从第6项的d-e测试,也可以验证输出电压设置为3.3V条件下,启动电流仍然是有限制的。
8.我的疑问是之前的分析是否正确,如果正确,应该如何解决这一问题。非常感谢!