输入dc5v,输出dc3.3v,请教一个参考电路实现该功能
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如果不限制使用61085,而是只完成5V到3.3v的隔离变换
不清楚你的要求的电流值
可以参见这个链接,有完整的原理图,BOM和测试结果
http://www.ti.com/tool/PMP5317?keyMatch=null&tisearch=tidesigns-power
This reference design provides isolated 7V, +3.3V, and -3.3V outputs at 100mW total power from a 2.6Vdc to 5.1Vdc input. With total power loss below 40mW, the full load efficiency is over 70%. The minimum load losses are kept below 25mW. The TPS43000 is used to control this multiple-output flyback converter. The entire circuit fits onto a 1 square inch, single-sided circuit board.
Hi
参考这个: http://www.ti.com.cn/cn/lit/an/slva496/slva496.pdf
TPS61085低成本隔离设计。