Other Parts Discussed in Thread: TPS51312, TPS563201, TPS563208
我板子上通过TPS51312实现3.3V、2.5V、1.8V、1.35V,输入电压都是5.0V,测试发现纹波很大,3.3V和2.5V的纹波达到80mV左右,1.8V和1.35V达到50mV左右,只要把各自电源的负载加到0.5A左右,输出纹波就很小,都能达到15mV左右,问题是我的板子上这些芯片的负载电流就是小;后面通过调大the fast feedforward capacitor(CFF)电容,由47pF调到0.1uF后,不加大负载的情况下,也可以把输出纹波跳到20mV左右,请问有什么好的解决方案吗,谢谢!具体原理图见附件