我按照BQ24298 的参考电路做了个充电电路同时当不间断电源的功能,可是 当断开电池后,后级系统部分只维持了一会儿就关闭了。请问这个充电IC, 如果在电池损坏情况下,移除电池后,这个SYS 输出端还会利用VBUS输入端来提供足够的电流供后面的系统使用吗?我的VBUS输入端接的是5v/3A 的电源。可以通过设定来取得SYS最大输出电流吗?还是需要选择其它的 IC来满足要求?后级系统要求4.2v/最大电流 2A。 谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.