This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27510-G3 低温下存储



我们一产品上使用的流量计芯片BQ27510-G3,电池满充后在做整机低温-40℃存储8小时后,取出后在常温下恢复,恢复时间大于4h,此时开机电池电量显示0%,测量电压为8.3V左右,重新插拔电池后电量显示正常为90%+,或者插上适配器进行充电后亦可恢复,帮忙分析下原因,谢谢!