This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2819 MOSFET 驱动问题

Other Parts Discussed in Thread: TPS2819

请问 TPS2819  MOS 驱动 芯片 的 电源用12VDC 时, 输入引脚IN 与MCU 连接(0-3.3V) , 输出OUT 是 0-12V 还是 与输入相等(0-3.3V)呢?  我现在想驱动MOSFET,开启电压最好在12V左右, 但是输入为逻辑电平3.3V, 是否可以直接用?

看到datasheet 上面写的 IN=OUT, 这里不太明白是 逻辑高或者底相等   还是 电压也相等?

  • HI

        驱动供电用的是VCC电压,所以驱动出来的电压是接近Vcc的(会有一定压降)

        

        驱动输入电平高输入门槛: (VCC12V,  3.3V输入明显是偏低的,你可以测试确认一下)