Other Parts Discussed in Thread: LM3409
输入您的问题:
您好,按照 datasheet的参考电路(如贴中电路所示),我用LM3409HVMY设计个一个0---1.24V的模拟调光驱动,原理图跟上图一样。设计电压输入为DC 24V,负载是一个成品LED灯(18并6串),输出电压Vo=19V,最大输出电流为560mA, 元件的选择如下:Cin1=22uF(50V),CF=1uF(50V),Coff=470pF(50V),CF2=0.1uF(50V),L1=100uH,Rsns=0.4欧,Ruv1=6.8K,Ruv2=50K,RF2=1K, D1为SR560,Q1为NTD20P06.
调试输入DC 24V时,LM3409HVMY和Q1(NTD20P06)的温度很高,输出电流是1A调节Rsns的电阻值电流值基本不变,IADJ脚加一个0到1.24V的电压不能调光。弄了一个星期了也不知道那里的问题,真不知道是那里的问题了。希望各位帮忙分析一下,谢了。