你好:我选用LMR16010做电源,输入16V,输出6.8V,测试的时候发现短路电流(输出端短路,测输入端电流)有点大,
请问哪位知道这个器件的大概短路电流?手册看了一遍没发现关于短路电流的问题。在线等,谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:我选用LMR16010做电源,输入16V,输出6.8V,测试的时候发现短路电流(输出端短路,测输入端电流)有点大,
请问哪位知道这个器件的大概短路电流?手册看了一遍没发现关于短路电流的问题。在线等,谢!
Hi
短路电流时会非常大,至少超过2.1A的电流限制。
一般datasheet不会说明短路电流这个参数,因为将输出短接到GND,电流时会很大的(Vo/R, R接近0),但是芯片会过流保护,所以会认为至少会大于过流保护点。
那这种过流保护产生的电流消耗在哪里了?电感?实测短路后电流有60-70ma,其他的DCDC芯片没发现有这么大,基本都忽略不计。
Hi
你所提到的60~70mA是指输入电流,而非短路时的负载电流。这个电流大小取决于芯片过载的控制方式。LMR16010是逐波峰值电流控制(过载时会i在降低频率的情况下不断的启动,再保护),会有输入电流消耗,主要消耗在功率器件上。
你所提到的很多芯片短路后无电流消耗(没有输入电流),这类芯片的过载保护方式是直接latch掉,即芯片会关闭不工作,自然不会有输入电流消耗。
The LMR16010 is protected from over current condition by cycle-by-cycle current limiting on the peak current of the high-side MOSFET. High-side MOSFET over-current protection is implemented by the nature of the Peak Current Mode control. T
The LMR16010 also implements a frequency fold-back to protect the converter in severe over-current or short conditions. The oscillator frequency is divided by 2, 4, and 8 as the FB pin voltage decrease to 75%, 50%, 25% of VREF.
Hi
不会。
保护也有各的好处。
Latch的好处是降低了损耗,但是恢复正常需要对芯片重启。
逐波保护,芯片是在不停重启,如果短路消失,芯片可自动正常供电。
你好,关于短路,你可以参考Datasheet的图29.图中显示的是短路时的电感电流情况,可以发现由于芯片在不断重启,所以输出是存在电流的,这是正常现象。
关于不断重启的保护,可以在短路消失的时候芯片自动恢复工作,不会像短路latch那样,需要重新上电才会恢复正常工作。但这种重启的保护方式有个小弊端就是会在保护期间带来能量的损耗以及温度的增加。