本人想将15V直流电压转为12V直流电压,采用LM25011方案,根据TI官网将反电阻比值算出,并是输出固定在12V,模拟也为12V,但是在实际电路中,输出为6.8V,我更换了反馈端电阻,输出值依旧不变,请问这是什么原因,有什么解决办法?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
将负载电流降低看能否保持12V输出? 如果可以,确认如下:
1. 功率电感饱和电流是否足够,建议必须大于最大输出电流的1.2倍。
2. 功率回路尽量小,layout尽量避免sense电阻的noise.
Hi
你可能测试的是用万用表,而非示波器。 即便是6.8V的输出,2个反馈电阻上的电压加起来也应该是6.8V,说明输出是不稳定的6.8V(上下震荡,万用表测得的示数不准确)
如之前回复的确认。 如果电流不大,说明很可能是layout问题,你测试sense电阻的波形即可以确认是否触发保护。