你好,在使用TPS60211按照典型电路搭建,出现如下的情况,在3.3V直流电源供电 用电流表检测电流,发现TPS60211电流功耗翻倍。求解
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,在使用TPS60211按照典型电路搭建,出现如下的情况,在3.3V直流电源供电 用电流表检测电流,发现TPS60211电流功耗翻倍。求解
Hi
问题只出在3.3V, 高一点或者低一点,输入电流都会降下去?
我觉得应该是低于3.3V时和高于3.3V是会出现输入电流差异的,因为前者是升压,后者是降压,芯片内部动作不应该一样,这将导致差异。
你好,我是用的是锂电池3.3V或3.7V电池对TPS60211进行供电输出3.3V,如用锂电池3.7V电池供电,手册上TPS60211的输入范围为1.8~3.6V这将对TPS60211有什么影响,此外芯片在3.3V和3.7V的的转换效率能达到多少。随着时间的增加锂电池电池的电压在不断降低,有没有适合锂电池电池使用的芯片一直能保持3.3V输出,效率也比较高的。谢谢
Hi
超过3.6V有烧芯片的风险,不建议选用这个方案。