制作的是10S铁电池, 满充-满放-满充,电量RSOC差不多准确了,但是FCC一直不更新。看资料更新条件还是没看懂,谁知道怎么回事。
9.1.6 Capacity Learning (FCC Update)
The bq78350-R1 updates FCC with an amount based on the value in DCR if a qualified discharge occurs.
The new value for FCC equals the DCR value plus the value of nearly full and low battery levels, as
shown in the following equation:
FCC (new) = DCR (final) = DCR (initial) + Measured Discharge to EDV2 + (FCC × Battery_Low%)
Where Battery_Low% = (Battery Low%) ÷ 2.56