我用的TPS40200产生的一个PWM波,电阻取了680k,电容取了560pF,SS引脚,FB引脚和ISNS引脚都没接,comp引脚给了一个小于1.4V的电平,上电后检测三角波正常,频率和理论值相近,但是输出的PWM波低电平有点类似锯齿波的样子,最低两伏左右,最高4V左右,而高电平正常为8V。由于我后级带了一个NPN管,这样输出的PWM低电平也会使三极管导通,这样就不正常了。请问是我没接的那几个引脚导致了上述问题么?请工程师解答。谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
测试一下你给的1.4V是否存在波动?另外驱动脚560pF改小到100pF电阻改到1k看看?
同时确保VDD电压稳定(用10uF电容靠近VDD 焊接用于稳压)
谢谢解答,还有我想问40200输出的PWM能直接输入给tps28225然后输出两路PWM供同步整流驱动么,我担心驱动能力不够,想在中间加三极管加大驱动能力。我看28225的datasheet,第一页的图中40200的输出是经过一个MOS管后再给28225的。
电阻改到1k有问题的吧,datasheet的12页有一个公式不是要Vin/R<=750uA
Hi
不存在驱动能力的问题,TPS28225需要的只是一个PWM电平信号,datasheet里面增加MOS的接口部分,我认为只是改变PWM启动逻辑。
驱动能力是在驱动大QgMOS时才需要的,PWM输入本身一般都是高阻抗,没有电流输入,当然就不需要较大驱动能力。
你说的改变逻辑应该是对的。不过40200产生的PWM好像就是有问题的,经过一个MOS管后就可以让高低电平无抖动。现在开环的电路已经做出来了,正在准备闭环。谢谢解答。